CMP#.WIDTHT
Description
CMP#.WIDTHT sets the time duration of the output pulse generated by the setpoint
Setpoint is the target value that an automatic control system, for example PID controller, will aim to reach. It is used when CMP#.WIDTHTYPE for the setpoint is set to 1.
It takes two command line arguments: the first specifies the setpoint, and the second specifies the time duration.
Examples
The following diagram illustrates CMP#.WIDTHT
.
Code
The following commands set the time widths of channel 1 setpoint 5 to 3.5 ms and channel 2 setpoint 1 to 20 ms.
--> CMP1.WIDTHTYPE 5 1
--> CMP1.WIDTHT 5 3.5
--> CMP2.WIDTHTYPE 1 1
--> CMP2.WIDTHT 1 20
Context
For more information please refer to Compare.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-06-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
ms |
|
Range |
0 to 1000.000 |
|
Default Value |
0 |
|
Data Type |
Float |
|
See Also |
|
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
CMP1.WIDTHT |
31460 |
7AE4 |
Unsigned32[8] |
Read/Write |
- |
|
CMP2.WIDTHT |
31461 |
7AE5 |
Unsigned32[8] |
Read/Write |
- |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
CMP1.WIDTHT |
31460 |
Float[8] |
Read/Write |
- |
|
CMP2.WIDTHT |
31461 |
Float[8] |
Read/Write |
- |